SA Bus Device Selection Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
See the Defining Hardware section.

Table 1. SA Bus Device Selection Dialog Box

Field

Description

Selections

Includes information for the following:
  • Name: Displays the names of the available selections.
  • Description: Description of the available selections.
  • Device Type: Type of controller.
  • Region: Displays the region of the controller.
  • Universal Inputs: Number of universal inputs.
  • Analog Inputs: Number of analog inputs.
  • Binary Inputs: Number of binary inputs.
  • Universal Outputs: Number of universal outputs.
  • Analog Outputs: Number of analog outputs.
  • Binary Outputs: Number of binary outputs.
  • Relay Outputs: Number of relay outputs.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.