Defining the Default Controller (Default Controller Tab) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

Use the Default Controller tab to select the default device when users select a specific system type in the System Selection Wizard.

Procedure

  1. Click Define Hardware. The Define Hardware dialog box appears.
  2. Click the Default Controller tab.
  3. For each application in the System Type column, select the default controller in the Default Controller column.