Modules (Custom/Monitoring Misc Temps) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Misc Temps selections load the following modules in this Control View column:

Inputs

  • CLRX-T (Cooler X Temperature AI, where X is 1-4): This Input is loaded when the Cooler Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • FZRX-T (Freezer X Temperature AI, where X is 1-4): This Input is loaded when the Freezer Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • POOL-T (Pool Temperature AI): This Input is loaded when the Pool Temperature Sensor (AI) node is selected.

See the Input Modules section.