Modules (Custom/Monitoring Command Motor) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Command Motor selections load the following modules in these Control View columns:

Inputs

  • MOTORX-S (Motor X Status BI, where X is 1-6): This Input is loaded when the Status (BI) node is selected. The Status (BI) node is available for selection when the Command Motor (BO) and one of the Quantity nodes are selected. Specific Inputs are loaded per motor.

See the Input Modules section.

Outputs

  • MOTORX-C (Motor X Command BO, where X is 1-6): This Output is loaded when the Command Motor (BO) and one of the Quantity nodes are selected. Specific Outputs are loaded per motor.

See the Output Modules section.