Modules (Custom/Monitoring Command Heat Tape) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Command Heat Tape selections load the following modules in this Control View column:

Outputs

  • HTAPEX-C (Heat Tape X Command BO, where X is 1-6): This Output is loaded when the Command Heat Tape (BO) node is selected. Specific Outputs are loaded per sensor.

See the Output Modules section.