Command Heat Tape (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The selection options for Command Heat Tape are:

  • Command Heat Tape (BO): This option is used to command heat tape to warm piping under freeze conditions for up to six locations.

    • 1 Output (BO)

    • 2 Outputs (2 BOs)

    • 3 Outputs (3 BOs)

    • 4 Outputs (4 BOs)

    • 5 Outputs (5 BOs)

    • 6 Outputs (6 BOs)