Specifying Local Controller Display settings - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
Controller Tool Help
- Product
- Controls > Control Tools > Controller Configuration Tool
- Document type
- User Guide
- Document number
- LIT-12011147
- Version
- 15.0
- Revision date
- 2022-11-18
Procedure
-
Start the tool and open the controller application.
-
Select the Display widget.
-
Click Edit.
-
Locate the Display Setup panel.
-
In the Display area, click the drop-down box to select a Contrast level value.
-
In the Display area, click the drop-down box to select a Backlight Intensity setting value.
-
Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.