Creating a new Display page - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget.
  3. Click Edit.
  4. Locate the Display Pages panel.
  5. In the Customize area, click Create Page (). The Create Page dialog box appears.
  6. Enter a customized page name. The new page appears as the last folder in the Display Pages tree.
    Note: The DIS1710 and DLK0350 setup allows up to 13 customized pages. Additional customized pages are not recognized by the device and do not appear accurately in the controller display.
  7. Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.