Viewing Controller Information - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
About this task

To view controller information for one or more controllers on the field bus in the Configuration mode:

Procedure

  1. On the Tools menu, select Online Operations. The Online Operations Wizard appears.
  2. Select a Connection Type: Supervisor Passthru, Bluetooth, MAP 4.2+/BACnet Router, ZigBee, or Direct Ethernet Connection.
  3. Enter Connection Parameters. SeeTransferring to a Computer for further information.
  4. Select a discovery process: MAC Address or Instance Number. If you select MAC Address, enter the device address. If you select Instance Number, enter the device BACnet instance number.

    For information on viewing information of a controller while it is being commissioned (Commissioning mode only), see the Commissioning a System section.