Selecting a Block from the Control Block Palette - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
About this task

The Control Block palette appears at the bottom of the left panel in the logic view, below the Activities tree. The Control Block palette does not appear when the Control View Connections option or a module category folder (for example, Output Control) in the Activities tree is selected.

To select a block from the Control Block palette:

Procedure

  1. Browse through the folders in the palette to locate the block. See the Logic View screen description in the User Interface section.
    Note: Or, use the Launch Wizard to locate and add one or more logic blocks. See Using the Launch Wizard.
  2. Drag and drop the block from the palette to the logic diagram in the right panel.