Reordering Inputs in a Command Hierarchy Block - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Procedure

  1. Double-click a Command Hierarchy block. The Details dialog box for the Command Hierarchy (Enum Output) or Command Hierarchy (Boolean Output) appears. See the Command Hierarchy (Enum Output or Boolean Output) section.
  2. Select the IO Modifications check box. The Reorder button appears ().
  3. Click . You can now reorder the inputs.
    Note: You cannot add or delete inputs once you enter reorder mode.
    Figure 1. Command Hierarchy - Reorder Inputs Mode

  4. Click next to an input, and then drag the row to a new location in the list. You can also click a column header to sort the entries in ascending or descending order.
  5. Click Apply. The left pane of the Command Hierarchy Details view updates to show the input reordering changes.
  6. Click Close.

Results