See the Logic Tab Screen description in the User Interface section.
For information on printing summary reports, see Printing Summary Reports in the User Interface section.
To print the logic diagram:
Print Preview
Click the Print Preview button in the Logic View toolbar. The Print Preview screen appears with the following options:
-
Print Setup
Note: The Print Setup dialog box contains a Page Setup button that allows you to change the orientation of the page from Portrait to Landscape and vice versa. -
Print
-
Zoom In
-
Zoom Out
-
Fit In Window
Click the Print button in the Logic View toolbar. The Print dialog box appears. Select the desired print settings and properties and click OK.