Disabling Peer-to-Peer Communication - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
About this task

To disable peer-to-peer communication:

Procedure

  1. View the details of the Network Input or Network Output.
  2. Click Edit.
  3. In the Peer Reference section, select the Peer to Peer Disabled option in the Object Identifier drop-down menu.
  4. Click Apply, and then click Close.