Changing a State Table Label - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Procedure

  1. Click the State Tables tab. The State Tables tab appears with the system’s state selection data populated within tables in the right pane, and the states in the left pane of the tab. The panes allow you to scroll both vertically and horizontally, keeping the first column visible. See the State Selection (State Tables Tab) screen section.
  2. Click Edit.
  3. Right-click the module name and select Change Table Label (a yellow table heading indicates a connected module, whereas an orange table heading is a module that is not connected). The Rename/Name dialog box appears.
  4. Type a name in the Name field.
    Note: We recommend leaving the label field empty so that dynamic naming may be used.
  5. Click OK.
  6. Click Apply.