Adding the Hybrid Activity to the State Tables - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Procedure

  1. Add a table to the State Tables according to the instructions in the Adding a Table to the State Selection Tables section. In the Create State Selection Table dialog box, be sure to create the State Selection Table with an enumeration set that matches the States Text attribute of the State output of the Hybrid Activity you are connecting.
  2. In the Control View, right-click the Hybrid Activity and select View Connections.
    Note: If no items appear in the Connections table, expose ports for connection. See Exposing Ports.
  3. Connect the inputs and outputs as desired, including the State output.