This topic explains how to implement the Output Override Monitoring feature.
Effective Command inputs monitor the current command and the priority of the current command to an output object and make these values available for use within the application. These values are currently used by the Override Monitoring feature that prevents PID logic blocks from winding up and tuning incorrectly when the actual control outputs are overridden.
Scenarios where you might want to add an Effective Command input for an output include:
-
when a system has more stages than are currently supported by the application. An example of this scenario is a unit with more than eight stages of cooling. This configuration requires that you manually add extra binary outputs for the additional stages. Then, you must replace the MSC 08 module with the appropriate MSC for the actual number of stages present in your application (up to 12 stages). To add override monitoring for the additional stages, you must add Effective Command inputs to match the new binary outputs you just added.
-
when you need to add a custom control loop. We recommended you select a Sideloop for a custom control loop. Even if the logic within the sideloop is not complete enough to meet the specification for your application, the override monitoring feature for the outputs is automatically added. Then, you can modify the logic that enables the control loop to meet the specification.
If a loop requires that you manually add an analog output, and you want to use the override monitoring feature, you must add an associated Effective Command input to the Miscellaneous Inputs column of the Control View to provide this feature.
To add an effective command input for an output:
- Add the output module. For detailed instructions on how to add an output to your application, see Adding an Output or Miscellaneous Output.
- Select and add the appropriate effective command miscellaneous input module using Table 1. For detailed instructions on how to add an input to your application, see Adding an Input or Miscellaneous Input.
On the left side of the table, identify the output you added in Step 1. The right side of the table indicates the criteria to use when adding the associated effective command miscellaneous input module. The table includes the following columns to help configure the input/output pair:
- Standard Name - Indicates the standard name of the module visible via the Rename dialog box.
- Name - Indicates the name of the module visible in the Output and Miscellaneous Input columns of the Control View after the module is added to the application. A value of N/A in this column indicates that there is no available input/output pair.
- Application - Indicates the Application filter to select in the Input Selection and Output Selection dialog boxes.
-
Function - Indicates the Function filter to select in the Input Selection and Output Selection dialog boxes.
To add more than one input/output pair, the output must have a unique standard name within the application (visible via the Rename dialog box).
- Verify that the Object Identifier of the miscellaneous input module matches that of the associated output module by viewing the Object Identifier attribute in the Details dialog box for both modules.
Output Configuration |
Miscellaneous Input Configuration |
||||||
---|---|---|---|---|---|---|---|
Standard Name | Name | Application | Function | Standard Name | Name | Application | Function |
2 Pipe Circulation Pump 1 BO | HCP1-C | 2 Pipe Circulation Pump 1 | Command | ||||
2 Pipe Circulation Pump 2 BO | HCP2-C | 3 Pipe Circulation Pump 2 | Command | ||||
Blr1 AO |
BLR1-O |
Boiler1 |
Output |
Eff Blr1 Cmd |
BLR1-% |
Blr1 |
Effective Command |
Blr1 BO |
BLR1-C |
Boiler1 |
Command |
N/A |
|||
Blr1 Pump AO |
BP1-O |
Boiler1 Circ Pmp |
Output |
Eff Blr1 Pump Cmd |
BP1-% |
Boiler1 Circ Pmp |
Effective Command |
Blr1 Pump BO |
BP1-C |
Boiler1 Circ Pmp |
Command |
N/A |
|||
Blr1 BO |
BLR1-EN |
Boiler1 Ena |
Command |
N/A |
|||
Blr1 Iso Valve BO |
BLR1ISOV-C |
Boiler1 Iso Valve |
Command |
N/A |
|||
Boiler 1 SP AO |
BLR1SP-O |
Boiler1 SP |
Output |
N/A |
|||
Blr2 AO |
BLR2-O |
Boiler2 |
Output |
Eff Blr2 Cmd |
BLR2-% |
Blr2 |
Effective Command |
Blr2 BO |
BLR2-C |
Boiler2 |
Command |
N/A |
|||
Blr2 Pump AO |
BP2-O |
Boiler2 Circ Pmp |
Output |
Eff Blr2 Pump Cmd |
BP2-% |
Boiler2 Circ Pmp |
Effective Command |
Blr2 Pump BO |
BP2-C |
Boiler2 Circ Pmp |
Command |
N/A |
|||
Blr2 BO |
BLR2-EN |
Boiler2 Ena |
Command |
N/A |
|||
Blr2 Iso Valve BO |
BLR2ISOV-C |
Boiler2 Iso Valve |
Command |
N/A |
|||
Boiler 2 SP AO |
BLR2SP-O |
Boiler2 SP |
Output |
N/A |
|||
Blr3 AO |
BLR3-O |
Boiler3 |
Output |
Eff Blr3 Cmd |
BLR3-% |
Blr3 |
Effective Command |
Blr3 BO |
BLR3-C |
Boiler3 |
Command |
N/A |
|||
Blr3 Pump AO |
BP3-O |
Boiler3 Circ Pmp |
Output |
Eff Blr3 Pump Cmd |
BP3-% |
Boiler3 Circ Pmp |
Effective Command |
Blr3 Pump BO |
BP3-C |
Boiler3 Circ Pmp |
Command |
N/A |
|||
Blr3 BO |
BLR3-EN |
Boiler3 Ena |
Command |
N/A |
|||
Blr3 Iso Valve BO |
BLR3ISOV-C |
Boiler3 Iso Valve |
Command |
N/A |
|||
Boiler 3 SP AO |
BLR3SP-O |
Boiler3 SP |
Output |
N/A |
|||
Blr4 AO |
BLR4-O |
Boiler4 |
Output |
Eff Blr4 Cmd |
BLR4-% |
Blr4 |
Effective Command |
Blr4 BO |
BLR4-C |
Boiler4 |
Command |
N/A |
|||
Blr4 Pump AO |
BP4-O |
Boiler4 Circ Pmp |
Output |
Eff Blr4 Pump Cmd |
BP4-% |
Boiler4 Circ Pmp |
Effective Command |
Blr4 Pump BO |
BP4-C |
Boiler4 Circ Pmp |
Command |
N/A |
|||
Blr4 BO |
BLR4-EN |
Boiler4 Ena |
Command |
N/A |
|||
Blr4 Iso Valve BO |
BLR4ISOV-C |
Boiler4 Iso Valve |
Command |
N/A |
|||
Boiler 4 SP AO |
BLR4SP-O |
Boiler4 SP |
Output |
N/A |
|||
Blr5 AO |
BLR5-O |
Boiler5 |
Output |
Eff Blr5 Cmd |
BLR5-% |
Blr5 |
Effective Command |
Blr5 BO |
BLR5-C |
Boiler5 |
Command |
N/A |
|||
Blr5 Pump AO |
BP5-O |
Boiler5 Circ Pmp |
Output |
Eff Blr5 Pump Cmd |
BP5-% |
Boiler5 Circ Pmp |
Effective Command |
Blr5 Pump BO |
BP5-C |
Boiler5 Circ Pmp |
Command |
N/A |
|||
Blr5 BO |
BLR5-EN |
Boiler5 Ena |
Command |
N/A |
|||
Blr5 Iso Valve BO |
BLR5ISOV-C |
Boiler5 Iso Valve |
Command |
N/A |
|||
Boiler 5 SP AO |
BLR5SP-O |
Boiler5 SP |
Output |
N/A |
|||
Blr6 AO |
BLR6-O |
Boiler6 |
Output |
Eff Blr6 Cmd |
BLR6-% |
Blr6 |
Effective Command |
Blr6 BO |
BLR6-C |
Boiler6 |
Command |
N/A |
|||
Blr6 Pump AO |
BP6-O |
Boiler6 Circ Pmp |
Output |
Eff Blr6 Pump Cmd |
BP6-% |
Boiler6 Circ Pmp |
Effective Command |
Blr6 Pump BO |
BP6-C |
Boiler6 Circ Pmp |
Command |
N/A |
|||
Blr6 BO |
BLR6-EN |
Boiler6 Ena |
Command |
N/A |
|||
Blr6 Iso Valve BO |
BLR6ISOV-C |
Boiler6 Iso Valve |
Command |
N/A |
|||
Boiler 6 SP AO |
BLR6SP-O |
Boiler6 SP |
Output |
N/A |
|||
Blr7 AO |
BLR7-O |
Boiler7 |
Output |
Eff Blr7 Cmd |
BLR7-% |
Blr7 |
Effective Command |
Blr7 BO |
BLR7-C |
Boiler7 |
Command |
N/A |
|||
Blr7 Pump AO |
BP7-O |
Boiler7 Circ Pmp |
Output |
Eff Blr7 Pump Cmd |
BP7-% |
Boiler7 Circ Pmp |
Effective Command |
Blr7 Pump BO |
BP7-C |
Boiler7 Circ Pmp |
Command |
N/A |
|||
Blr7 BO |
BLR7-EN |
Boiler7 Ena |
Command |
N/A |
|||
Blr7 Iso Valve BO |
BLR7ISOV-C |
Boiler7 Iso Valve |
Command |
N/A |
|||
Boiler 7 SP AO |
BLR7SP-O |
Boiler7 SP |
Output |
N/A |
|||
Blr8 AO |
BLR8-O |
Boiler8 |
Output |
Eff Blr8 Cmd |
BLR8-% |
Blr8 |
Effective Command |
Blr8 BO |
BLR8-C |
Boiler8 |
Command |
N/A |
|||
Blr8 Pump AO |
BP8-O |
Boiler8 Circ Pmp |
Output |
Eff Blr8 Pump Cmd |
BP8-% |
Boiler8 Circ Pmp |
Effective Command |
Blr8 Pump BO |
BP8-C |
Boiler8 Circ Pmp |
Command |
N/A |
|||
Blr8 BO |
BLR8-EN |
Boiler8 Ena |
Command |
N/A |
|||
Blr8 Iso Valve BO |
BLR8ISOV-C |
Boiler8 Iso Valve |
Command |
N/A |
|||
Boiler 8 SP AO |
BLR8SP-O |
Boiler8 SP |
Output |
N/A |
|||
Box Heating 2 Position BO |
HTG-C |
Box Heating |
Command |
Eff Box Heating 2 Position Binary Cmd |
HTG-EC |
Box Heating 2 Position |
Effective Vlv Command |
Box Heating Stage 1 BO |
HTG1-C |
Box Heating |
Stage 1 Command |
Eff Box Heating Stage 1 Binary Cmd |
HTG1-EC |
Box Heating Stage 1 |
Effective Stg Command |
Box Heating Stage 2 BO |
HTG2-C |
Box Heating |
Stage 2 Command |
Eff Box Heating Stage 2 Binary Cmd |
HTG2-EC |
Box Heating Stage 2 |
Effective Stg Command |
Box Heating Stage 3 BO |
HTG3-C |
Box Heating |
Stage 3 Command |
Eff Box Heating Stage 3 Binary Cmd |
HTG3-EC |
Box Heating Stage 3 |
Effective Stg Command |
Box Heating Valve AO |
HTG-O |
Box Heating |
Output |
Eff Box Heating Valve Cmd |
HTG-% |
Box Heating |
Effective Command |
Box Heating Valve PAO |
HTG-O |
Box Heating |
Output_PAO |
Eff Box Heating Valve Cmd |
HTG-% |
Box Heating |
Effective Command |
Box Heating Enable BO |
HTG-EN |
Box Heating Enable |
Command |
N/A |
|||
HW Bypass Valve AO |
BYPV-O |
Bypass Loop |
Output |
Eff HW Bypass Valve Cmd |
BYPV-% |
HW Bypass Valve |
Effective Command |
Calibration Solenoid BO |
ACSOL-C |
Calibration |
Command |
N/A |
|||
Chiller 1 CHW Iso Valve BO |
CH1CHWISOV -C |
Chiller 1 CHW Iso Valve |
Command |
N/A |
|||
Chiller 1 CW Iso Valve BO |
CH1CWISOV-C |
Chiller 1 CW Iso Valve |
Command |
N/A |
|||
Chiller 2 CHW Iso Valve BO |
CH2CHWISOV-C |
Chiller 2 CHW Iso Valve |
Command |
N/A |
|||
Chiller 2 CW Iso Valve BO |
CH2CWISOV-C |
Chiller 2 CW Iso Valve |
Command |
N/A |
|||
Chiller 3 CHW Iso Valve BO |
CH3CHWISOV-C |
Chiller 3 CHW Iso Valve |
Command |
N/A |
|||
Chiller 3 CW Iso Valve BO |
CH3CWISOV-C |
Chiller 3 CW Iso Valve |
Command |
N/A |
|||
Chiller 4 CHW Iso Valve BO |
CH4CHWISOV-C |
Chiller 4 CHW Iso Valve |
Command |
N/A |
|||
Chiller 4 CW Iso Valve BO |
CH4CWISOV-C |
Chiller 4 CW Iso Valve |
Command |
N/A |
|||
Chiller 5 CHW Iso Valve BO |
CH5CHWISOV-C |
Chiller 5 CHW Iso Valve |
Command |
N/A |
|||
Chiller 5 CW Iso Valve BO |
CH5CWISOV-C |
Chiller 5 CW Iso Valve |
Command |
N/A |
|||
Chiller 6 CHW Iso Valve BO |
CH6CHWISOV-C |
Chiller 6 CHW Iso Valve |
Command |
N/A |
|||
Chiller 6 CW Iso Valve BO |
CH6CWISOV-C |
Chiller 6 CW Iso Valve |
Command |
N/A |
|||
Chiller 7 CHW Iso Valve BO |
CH7CHWISOV-C |
Chiller 7 CHW Iso Valve |
Command |
N/A |
|||
Chiller 7 CW Iso Valve BO |
CH7CWISOV-C |
Chiller 7 CW Iso Valve |
Command |
N/A |
|||
Chiller 8 CHW Iso Valve BO |
CH8CHWISOV-C |
Chiller 8 CHW Iso Valve |
Command |
N/A |
|||
Chiller 8 CW Iso Valve BO |
CH8CWISOV-C |
Chiller 8 CW Iso Valve |
Command |
N/A |
|||
Chlr1 BO |
CH1-EN |
Chiller1 |
Command |
N/A |
|||
Chlr1 CHW ISO Valve AO |
CH1CHWISOV-O |
Chiller1 CHW Iso Valve |
Output |
N/A |
|||
Chlr1 CHW Iso Valve BO |
CH1CHWISOV-C |
Chiller1 CHW Iso Valve |
Command |
N/A |
|||
Chlr1 Curr Limit AO |
CH1CL-O |
Chiller1 CurrLim |
Output |
Eff Chlr1 Curr Limit Cmd |
CH1CL-% |
Chlr1 Curr Limit |
Effective Command |
Chlr1 CW ISO Valve AO |
CH1CWISOV-O |
Chiller1 CW Iso Valve |
Output |
N/A |
|||
Chlr1 CW Iso Valve BO |
CH1CWISOV-C |
Chiller1 CW Iso Valve |
Command |
N/A |
|||
Chlr1 Setpoint AO |
CH1SP-O |
Chiller1 Setpoint |
Output |
Eff Chlr1 Setpoint Cmd |
CH1SP-% |
Chlr1 Setpoint |
Effective Command |
Chlr2 BO |
CH2-EN |
Chiller2 |
Command |
N/A |
|||
Chlr2 CHW ISO Valve AO |
CH2CHWISOV-O |
Chiller2 CHW Iso Valve |
Output |
N/A |
|||
Chlr2 CHW Iso Valve BO |
CH2CHWISOV-C |
Chiller2 CHW Iso Valve |
Command |
N/A |
|||
Chlr2 Curr Limit AO |
CH2CL-O |
Chiller2 CurrLim |
Output |
Eff Chlr2 Curr Limit Cmd |
CH2CL-% |
Chlr2 Curr Limit |
Effective Command |
Chlr2 CW ISO Valve AO |
CH2CWISOV-O |
Chiller2 CW Iso Valve |
Output |
N/A |
|||
Chlr2 CW Iso Valve BO |
CH2CWISOV-C |
Chiller2 CW Iso Valve |
Command |
N/A |
|||
Chlr2 Setpoint AO |
CH2SP-O |
Chiller2 Setpoint |
Output |
Eff Chlr2 Setpoint Cmd |
CH2SP-% |
Chlr2 Setpoint |
Effective Command |
Chlr3 BO |
CH3-EN |
Chiller3 |
Command |
N/A |
|||
Chlr3 CHW ISO Valve AO |
CH3CHWISOV-O |
Chiller3 CHW Iso Valve |
Output |
N/A |
|||
Chlr3 CHW Iso Valve BO |
CH3CHWISOV-C |
Chiller3 CHW Iso Valve |
Command |
N/A |
|||
Chlr3 Curr Limit AO |
CH3CL-O |
Chiller3 CurrLim |
Output |
Eff Chlr3 Curr Limit Cmd |
CH3CL-% |
Chlr3 Curr Limit |
Effective Command |
Chlr3 CW ISO Valve AO |
CH3CWISOV-O |
Chiller3 CW Iso Valve |
Output |
N/A |
|||
Chlr3 CW Iso Valve BO |
CH3CWISOV-C |
Chiller3 CW Iso Valve |
Command |
N/A |
|||
Chlr3 Setpoint AO |
CH3SP-O |
Chiller3 Setpoint |
Output |
Eff Chlr3 Setpoint Cmd |
CH3SP-% |
Chlr3 Setpoint |
Effective Command |
Chlr4 BO |
CH4-EN |
Chiller4 |
Command |
N/A |
|||
Chlr4 CHW ISO Valve AO |
CH4CHWISOV-O |
Chiller4 CHW Iso Valve |
Output |
N/A |
|||
Chlr4 CHW Iso Valve BO |
CH4CHWISOV-C |
Chiller4 CHW Iso Valve |
Command |
N/A |
|||
Chlr4 Curr Limit AO |
CH4CL-O |
Chiller4 CurrLim |
Output |
Eff Chlr4 Curr Limit Cmd |
CH4CL-% |
Chlr4 Curr Limit |
Effective Command |
Chlr4 CW ISO Valve AO |
CH4CWISOV-O |
Chiller4 CW Iso Valve |
Output |
N/A |
|||
Chlr4 CW Iso Valve BO |
CH4CWISOV-C |
Chiller4 CW Iso Valve |
Command |
N/A |
|||
Chlr4 Setpoint AO |