Rename (Module/Block) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Use this dialog box to make changes to the labels in the block's name. See Renaming a Module and Renaming a Block.

Table 1. Rename (Module/Block)

Field

Description

User Name

Specify a name for the module/block.
Note: If this field is blank, the Standard Name is used.

Standard Name

Displays a Johnson Controls standard name for the module/block.

OK

Applies the name change and closes the dialog box. The name change appears in the Control View or Logic View.

Cancel

Closes the dialog box without applying the change.

Opens the Help system.