Online Operations Wizard - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
See the Viewing Controller Information section. The Online Operations Wizard contains the same device connection information as the Commissioning Device Wizard, with the addition of the Activate pending files, Enable logic, and Disable logic features. Use these features to: (a) control when transferred files are activated on the controller, and (b) modify the runtime logic of applications in a device.

For information about viewing a controller's information while it is being commissioned (Commissioning mode only), see the Commissioning a System section.

Table 1. Online Operations Wizard

Field

Description

Name

Name of the controller.

Command Command issued to the controller.
Status Status of the controller.

Description

Description of the controller.

Model

Model number of the controller.

Maincode Version

Firmware version of the controller.

Bootcode Version

Bootcode version of the controller.

System Name

System name of the controller.

Instance Number (BACnet ID)

BACnet ID number. This value is the same value used in the Peer Reference attribute in the Details View.

CPU Usage%

CPU usage of the controller.

Object Memory Usage%

Memory usage of the controller.

Radio Firmware Version 1

Firmware version of the wireless device.

Radio IEEE Address1

IEEE address of the wireless device.

Unbound References

Unbound references of the device.

Pan Id1

Pan ID of the wireless device.

Device Address

Device address of the controller.

Controller Number1 Combined value of the rotary switches or DIP switches on the device.

Logic Enabled

Logic status of an application configured in Transfer to Device (Download) . A status of True indicates that the logic of an application is enabled; a status of False indicates that the logic of an application is disabled. To modify the Logic Enabled status, select the Enable logic or Disable logic options in the Select an action list.

Note: The logic options do not take effect on the controller until the application is activated.

Background Transfer Status

Status of an application transferred using the Transfer to Device (Download) option. A status of Idle indicates that the application is activated in the controller; a status of Files are Staged indicates that the application has yet to be activated. Select Activate pending files in the Select an action list to activate transferred files.

Computer Name 2 Network hostname of the device.
DHCP Enabled2 Displays whether DHCP is enabled or not for devices.

When the DHCP is disabled, the static IP fields are editable.

IP Address2 IP Address for the device.
IP Mask2 Subnet mask used for the IP address.
IP Router Address2 IP address of the router for the device.
BBMD Enabled Displays the Enabled status of the Broadcast Management (BBMD) object. You can configure BBMD status in the Advanced tab. For further information, see Broadcast Management (BBMD) Object Screen.

Opens the Help system.

Table 2. Actions

Field

Description

Activate pending files

On supported devices, activates files that you transfer using the Wait for manual activation option. For further information, see Transferring to a Device.

Show diagnostic log

Opens the device error log for a selected controller. Diagnostic information is provided for troubleshooting advanced issues with your field support representative.
Enable logic On supported devices, enables the runtime logic of applications in a device.
Disable logic On supported devices, disables the runtime logic of applications in a device.
Note: You can view and modify the status of the logic value during device commissioning by clicking on the System Info link in the status bar. See System Information Details Dialog for more information.

SA Bus Status

Click this option to view the status of all SA Bus devices. See Transfer to Device Wizard for more information.

Perform Action Performs the action specified in the adjoining dropdown-list.

Copy to Clipboard

Copies the device's data to the clipboard for pasting into another program.

Refresh

Refreshes the result screen allowing user to re-query controller status.

1 This field contains data only when wirelessly connected.
2 Appears only for IP devices.
3 Appears only on compatible models.