See Configuring the Translation Blocks.
Field |
Description |
---|---|
Edit | Use to edit the table data. |
IO Modifications | Enables you to add, remove, or reorder inputs that define the columns in the table in the left pane. |
Name | Use to enter a name for the block. |
Object Identifier | Indicates object BACnet ID and instance number. |
Input and Outputs Table |
Displays both an Inputs and an Outputs table for the selected module/block. These tables include the following data:
|
Input (Orange Column Headers) |
Indicates the name of the input in which the column is associated. |
|
Use to drag inputs to reorder the input list. |
State Column (Turquoise Column Headers) |
Lists the output states of the commands in its rows. |
Table Rows (White with Text or Shaded with Asterisks) |
White table rows with text indicate the enumeration state or True/False state that is associated with the input column. Shaded table rows with asterisks indicate that the Translation module accepts any value for the input. |
Up and Down Arrows |
Moves the row up or down. |
Apply |
Applies the changes. |
Cancel |
Discards the changes. |
Close | Closes the screen. |
|
Opens the Help system. |