Rename/Name - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This dialog box is used to make changes to the labels in the State Tables. See Customizing State Selection Tables.

Table 1. Rename/Name Dialog

Field

Description

Name

Use to type a name for the input. We recommend leaving this field empty so that dynamic naming may be used.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.