MUX - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
See Configuring the MUX Block.

Table 1. MUX

Field

Description

Edit Use to edit the table data.
IO Modifications Enables you to add or remove inputs and outputs that define the modes buttons in the left pane.
Name Use to enter a name for the block.
Object Identifier Indicates object BACnet ID and instance number.
Input and Outputs Table

Displays both an Inputs and an Outputs table for the selected module/block. These tables include the following data:

  • Name: Name of the input or output.
  • Standard Name: Johnson Controls standard name used for the input or output.
  • Default Value: Input that is passed to the Present Value if the Mode value is not assigned to an input.
  • Units: Units of measurement used for the inputs and outputs and the States text for the enum inputs and outputs.
  • Display Precision: Display Precision value used for the inputs and outputs (for example, 10ths).
  • BACnet Exposed: Indicates whether the input or output parameter is exposed for BACnet systems.

Input 1 - Mode(s)

Defines the modes that are configured for this input. If the mode value equals one of the input mode configurations, the value on the input is passed. See Mode Selection.

Input 2 - Mode(s) 1

Defines the modes that are configured for this input. If the mode value equals one of the input mode configurations, the value on the input is passed. See Mode Selection.

Apply

Applies the changes.

Cancel

Discards the changes.

Close Closes the screen.

Opens the Help system.

1 The number of Input X - Mode(s) fields is determined by the number selected in the Input field.