Clone Ports Dialog - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Clone Ports dialog allows you to duplicate ports of a block. Only ports that are exposed and not connected can be duplicated; you cannot duplicate ports that are both exposed and connected. See the Cloning a Port section.

Table 1. Clone Ports Dialog

Field

Description

Input Port List

Lists the input ports you can duplicate.

Output Port List

Lists the output ports you can duplicate.

Select All

Selects the check boxes of all input/output ports in the Input Port List and Output Port List.

Deselect All

Clears the check boxes of all input/output ports in the Input Port List and Output Port List.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.