System Types and Configurations - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
When selecting a system, you first choose the overall type of system and a specific configuration to create. For example, you may select VAV as the system type and Single Duct as the specific configuration to use. See the Selecting a System (Creating a New System) steps and the Applications section for details on the System Selection options: