Adding a Trend - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
About this task

A trended item is a data point in the controller that is periodically sampled and logged. You can view trend logs in table or chart format. To view trend samples, you need to be in Commissioning mode.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, right-click Trends and then click Add Trend. A new trend is added to the Advanced Object tree.
  4. Select the trend and then click Edit. The fields you can edit appear in white.
  5. Enter information for the trend. See Trend Details Screen.
  6. Click Apply.