Viewing Event Logs - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
About this task

You can perform this task only in Commissioning mode.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree under Intrinsic Alarming, click Event Log and then click the Events tab. A list of events appear.
    Note:

    Click the columns to sort the list of events.

    To copy details from the event into another program, select the row and click Copy to Clipboard.

    To refresh the screen, click the lightning button on top left of the Events tab.