Viewing Device Information - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
To view Device Information, complete the following steps:

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. Under the Device Information folder, select the controller you want to view. Information about the controller (such as the controller name and the time zone) appears in the right section of the screen.