Adding a Calendar with a Date Range - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
About this task

You can add a calendar with a date range of exception days. For example, you may want to add an entire month (for example, summer hours) or a calendar that includes only Fridays (building closes early).

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab. The Advanced Object tree and information screen appear.
  3. In the Advanced Object tree, right-click Calendars and click Add Calendar. A new calendar is added to the Advanced Object tree.
  4. Click the calendar located below Calendars in the Advanced Object tree.
  5. Click Edit. The fields you can edit appear in white.
  6. Enter basic information for the calendar. See Calendar Details Screen.
  7. Next to the Date List field, click Add. The Calendar View window appears.
  8. Click Entry Detail. The Calendar Entry Detail screen appears. See Calendar Entry Detail Screen.
  9. Click New. In the Calendar Entry Detail screen, you can select one day, define a date range, or select an entire week.
  10. To select a date range, click Date Range, and then select your parameters in the To and From fields.
  11. To select an entire week (for example, the last week of December in every year), click Week and Day, and then select your parameters in the Month and Date fields.
  12. Click OK.
  13. Click Save.
  14. Click Apply.