Trend Viewer Chart View - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Chart view allows you to view data samples in chart format. You can zoom in, zoom out, and pan within the chart.

Table 1. Chart View (Commissioning Mode Only)

Button

View

Description

Update

Retrieves the most recent data samples for the displayed trends.

Zoom

Toggles the mouse behavior for the chart between zoom mode and normal mode.

While in zoom mode:

  • drag the mouse over an area of the chart to zoom in
  • left-click to zoom out one level
  • click Zoom to exit zoom mode and restore the mouse to normal mode

When you exit zoom mode, the chart remains at the current zoom level. Use the Restore button to fully zoom out.

Notes:
  • You cannot pan while the mouse is in zoom mode.
  • You can also zoom in and out in normal mode by using the Shift key and the mouse. To zoom, hold the Shift key while dragging the mouse across the chart. To zoom out one level, left-click the mouse while holding the Shift key down.

Restore

Use to return to a zoomed out view and switches the mouse back to normal mode when the chart's zoom mode is active.

Points Line

Data using lines and point markers. This is the default behavior.

Area

Data using an area chart.

Bar

Data using a bar chart.

Note: Use the bar chart only when the number of data samples can reasonably be expected to display as bars. If too many data samples exist when you click this option, the display becomes unstable and fails to properly update the screen. To recover, select any other display option.

Points

Data using markers with no lines.

Line

Data using lines with no markers.

Stacked Y Axis

Displays each trend on a separate Y axis. This option is not available when viewing a single trend.

Single Y Axis

Displays each trend with the same Y axis. This option is not available when viewing a single trend.