Define New Events Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

See Adding a Weekly Schedule.

Table 1. Define New Events Screen

Field

Description

Monday - Sunday

Use to select the days of the week for a schedule.

Mon-Fri

Use to select Monday through Friday for a schedule.

All

Use to select all days of the week.

Hour, Minutes

Indicates the time of the day you want to schedule.

Value

Indicates the default value that appears (for example, on or occupied) for the time frame you select. For example, yellow can indicate On, and blue can indicate Off.

OK

Saves changes to the information in the screen.

Cancel

Exits the screen without saving changes

Opens the Help system.