For information on how to view, edit, and add a Broadcast Management object, see Working with a Broadcast Management (BBMD) Object.
Field |
Description |
---|---|
Object | |
Name |
Indicates the name of the Broadcast Management object. |
Description |
Provides a basic description of the Broadcast Management object. |
Object Identifier |
Indicates the BACnet object ID for the Broadcast Management object. |
Enabled |
Select True or False to disable or enable BBMD functionality. This selection can be configured in the Transfer Summary screen. See Transfer to Device (Download).
Note: Enable only one device as a BBMD on a given subnet. If you do not know how to configure a BBMD, do not enable BBMD in your application or device. For further information, refer to the Metasys IP Networks for BACnet/IP Controllers Configuration Guide Technical Bulletin (LIT-12012468) .
|
Network | |
BM Address List |
Use this attribute to configure the endpoints that communicate with the BBMD. To view or edit this list see Viewing a Broadcast Management (BBMD) Object and Editing a Broadcast Management (BBMD) Object. |
Broadcast Disabled |
Indicates the broadcast status. |