Restoring Flow - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. In the details view of the Balancer Override SD module, click Flow Restore. The Flow Restore Command dialog box appears asking if you want to send the restore flow command.
  2. Click Send.

    Return to the Using the Balancing Feature section.