The following steps describe a typical use of the balancing feature:
-
Start the Test mode. See Starting the Test Mode.
-
Edit the VAV Box Controller balancing attributes such as Flow Setpoints to the desired values, if necessary. See Editing the Balancing Attributes.
-
Autocalibrate the VAV Box Controller. See Autocalibrating the VAV Box Controller.
-
Issue a Flow Override command to measure the flow in the space (for example, drive the VAV Box Controller to the maximum cfm). See Issuing a Flow Override Command.
-
If the flow measurement is accurate, restore the flow as-is. See Restoring Flow.
-
If the flow measurement is inaccurate, calculate the K-Factor with the new measurement. See Calculate K-Factors Command Dialog Box.
-
-
Exit the Test mode. See Stopping the Test Mode.