Making a Direct Ethernet Connection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  1. Open the tool.
  2. Click Commission. The Commission Device Wizard appears.
  3. Make your application and connection attribute selections and click Next.
  4. Select the device and click Next. The Commission Device Summary dialog box appears.
    Notes:
    • Verify you are on the same subnet as your IP controllers to use a Direct Ethernet connection.
    • If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.