See the Viewing Online Operations section.
For information on viewing Online Operations from the Configuration mode, see the Configuring a System section.
Field |
Description |
---|---|
Computer Name 1 | Network hostname of the device. |
Instance Number |
BACnet ID number. |
DHCP Enabled1 | Displays whether DHCP is enabled for the device. |
IP Address1 | IP Address for the device. |
IP Mask1 | Subnet mask used for the IP address. |
IP Router Address1 | IP address of the router for the field device. |
BBMD Enabled | Displays the Enabled status of the Broadcast Management (BBMD) object. You can configure this in the Advanced tab. For further information, see Broadcast Management (BBMD) Object Screen. |
Controller Number 2 | Combined value of the rotary switches or DIP switches on the device. |
Name |
Name of the controller. |
Description |
Description of the controller. |
Model |
Model number of the controller. |
Bootcode Version |
Bootcode version of the controller. |
Maincode Version |
Maincode version of the controller. |
System Name |
System name of the controller. |
CPU Usage |
CPU usage of the controller. |
Object Memory Usage |
Memory usage of the controller. |
Status |
Status of the controller. |
Radio Firmware Version 3 |
Firmware version of the wireless device. |
Radio IEEE Address3 |
IEEE address of the wireless device. |
Device Address |
Device address of the controller. |
Unbound References |
Unbound references of the device. |
FC Communication Mode | On compatible devices, indicates the following field bus communication: N2 Subordinate, Wired, Wireless, and Ethernet. |
Pan Offset3 |
Pan ID of the wireless devices. |
Logic Enabled |
Logic status of an application configured in Transfer to Device (Download) . A status of True indicates that the logic of an application is enabled; a status of False indicates that the logic of an application is disabled. To modify the Logic Enabled status, see Online Operations. Note: The logic options do not take effect on the controller until the application is activated.
|
Background Transfer Status |
Status of an application transferred using the Transfer to Device (Download) option. A status of Idle indicates that the application is activated in the controller; a status of Files are Staged indicates that the application has yet to be activated. To activate pending files, see Online Operations. |
SA Bus Status |
Click this option to view the status of all SA Bus devices. See Transfer to Device Wizard for more information. |
Refresh |
Updates the Online Operations Wizard. |
Close |
Closes the Online Operations Wizard. |
Field |
Description |
---|---|
Show diagnostic log |
Opens the device error log for a selected controller. Diagnostic information is provided for troubleshooting advanced issues with your field support representative. |
Enable logic | On supported devices, enables the runtime logic of applications in a device. |
Disable logic | On supported devices, disables the runtime logic of applications in a device.
Note: To view and modify the status of the logic value during device commissioning, click on the System Info link in the status bar. See System Information Details Dialog for more information.
|
Perform Action | Performs the action specified in the adjoining list. |
Refresh |
Refreshes the result screen allowing user to re-query controller status. |
Close |
Closes the wizard. |