Boiler Options (CH) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Use this section for miscellaneous boiler options.

The selection options for Boiler Options are:

  • Boiler Status: This option monitors the status of the boiler.

  • Boiler General Alarm: This option monitors the general alarm status of the boiler.

  • Boiler High Temp Alarm: This option monitors the high temperature alarm status of the boiler.

  • Boiler Flow Switch: This option monitors the flow switch status of the boiler.

  • Combustion Air Damper: This option controls a combustion air damper for the boilers.

    • End Switch: This option monitors the Combustion air damper status.

  • Hot Water Supply Temp Per Boiler: This option monitors the leaving (or supply) water temperature of each boiler.

  • Hot Water Return Temp Per Boiler: This option monitors the entering (or return) water temperature of each boiler.

  • Isolation Valves on each Boiler: This option controls an isolation valve for each boiler.

    • Valve Open Status: This option monitors the isolation valve status.

  • Main Steam Header Pressure: This option monitors the steam pressure of the system.

If the Hot Water/Steam Boilers is not selected, none of these options can be selected.

If the Pressure (Steam Boilers) is selected, the Main Steam Header Pressure cannot be selected.

If the Pressure (Steam Boilers) or Dedicated Boiler Pump(s) is selected, the Isolation Valves on each Boiler cannot be selected.