Cooling System Enable (CC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The selection option for Cooling System Enable is:

  • OA Cooling Lockout: This input is the setpoint, below which, the system is locked out or disabled.

  • Emergency Shutdown: This option allows the system to automatically shut down upon activation of a binary input.

  • Low Pressure Shutdown: This option allows the system to automatically shut down should the system pressure drop below a specified pressure.