Chiller Options (CC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The selection options for Chiller Options are:

  • Chilled Water Options - Per Chiller

    • Flow Switch: This option monitors the flow switch status of the chiller.

    • Flow Sensor: This option monitors the flow sensor of the chiller.

    • Entering Water Temp: This option monitors the entering (return) water temperature of each chiller.

    • Leaving Water Temp: This option monitors the leaving (supply) water temperature of each chiller.

    • Isolation Valve: This option controls an isolation valve for each chiller.

      • Valve Open Status: This option monitors the isolation valve status.

  • Condenser Water Options - Per Chiller

    • Flow Switch: This option monitors the flow switch status of the chiller.

    • Flow Sensor: This option monitors the flow sensor of the chiller.

    • Entering Water Temp: This option monitors the entering or return water temperature of each chiller.

    • Leaving Water Temp: This option monitors the leaving or supply water temperature of each chiller.

    • Isolation Valve: This option controls an isolation valve for each chiller.

      • Valve Open Status: This option monitors the isolation valve status.

  • Chiller Alarm(s): This option monitors the general alarm status of the chiller.

  • Chiller Setpoint Adjustment(s): This option generates an AO to each chiller to command the setpoint through the BAS.

  • Chiller Current Limit Adjustment(s): This option generates an AO to each chiller to command the current limit through the BAS.

  • Chiller Amperage(s): This option monitors the chiller amperages of each chiller.

  • Primary Supply Temperature: This option monitors the primary supply water temperature.

  • Primary Return Temperature: This option monitors the primary return water temperature.

  • Primary Flow Sensor: This option monitors the primary flow sensor.

  • Refrigerant Monitor Panel Alarm: This option monitors the refrigerant monitor panel alarm.