The Central Plant applications provide selections capable of controlling many different heating and cooling configurations. The mechanical system and control logic selections for the Central Plant applications are integrated into the Mechanical System Selection screen of the System Selection Wizard. Input sensors are automatically loaded if they are required for a selected device or control option. The Control Logic Selection screen provides optional sensors, equipment, and monitored safeties.
When you press F1 or click the Help icon, a feature description and associated modules appear on the right side of the screen, as you highlight each selection in the tree.
See the sections specific to the Central Plant Application Type:
See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.