Parallel Primary CW Pumps (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
In the following figure, the condenser water pumps are connected in a headered or parallel configuration so that any pump may be used with any chiller. The isolation valves are piped to the chillers in a dedicated configuration to prevent water from flowing through an inactive chiller.

Figure 1. Water-Cooled Condenser Headered System