Secondary Chill Water Options (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The selection options for Secondary Chill Water Options are:

  • Supply Temperature: This option monitors the secondary loop supply temperature.

  • Return Temperature: This option monitors the secondary loop return temperature.

  • Flow Meter: This option monitors the secondary loop flow rate.

  • Decouple Temperature: This option monitors the decouple loop temperature.

  • Decouple Flow Meter: This option monitors the decouple loop flow rate.

  • Decouple Flow Direction: This option monitors the decouple loop flow direction.

  • Building Load Meter: This option monitors the secondary loop BTUs.