Heat Exchanger Options (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The selection options for Heat Exchanger Options are:

  • Chilled Water Options - Per Heat Exchanger

    • Flow Switch: This option monitors the flow switch status of the heat exchanger.

    • Flow Sensor: This option monitors the flow sensor of the heat exchanger.

    • Entering Water Temp: This option monitors the entering (return) water temperature of each heat exchanger.

    • Leaving Water Temp: This option monitors the leaving (supply) water temperature of each heat exchanger.

  • Condenser Water Options - Per Heat Exchanger

    • Flow Switch: This option monitors the flow switch status of the heat exchanger.

    • Flow Sensor: This option monitors the flow sensor of the heat exchanger.

    • Entering Water Temp: This option monitors the entering or return water temperature of each heat exchanger.

    • Leaving Water Temp: This option monitors the leaving or supply water temperature of each heat exchanger.

  • Heat Exchanger Alarm(s) and outputs: These options monitors the general alarm status of the heat exchanger.