Basin Options (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The selection options for Basin Options are:

  • Dedicated - one per tower: This option provides control if all the towers have individual basins.

  • Common Sump: This option provides control if all the towers share a common basin.

  • Basin Level Alarm(s): This option monitors basin low level alarms.

  • Basin Heater Enable(s): This option generates BOs to command the basin heaters through the BAS.

  • Basin Water Temperature(s): This option monitors basin water temperatures.

    • Switch(es): This option monitors BI inputs for low temperature switches.

    • Analog Temperature(s): This option monitors AI inputs for temperature.

  • Basin Level Switch(es): This option monitors the basin levels.

  • Basin Makeup Valve(s): This option generates BOs to command basin makeup valves through the BAS.

If the No CW Piping (Air Cooled) node is selected, Basin Options cannot be selected.