Box Flow Test Overview - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Use the Box Flow Test to verify and diagnose the operation of Single Duct, Dual Duct, and Supply Exhaust applications. The Box Flow Test module provides the timing, output control, and data-gathering functions for testing the flow control performance of a VAV Box Controller application.

See Box Flow Test in the State Generators section for information on the Box Flow Test module.