Binary Value Commands - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Table 1 describes the Binary Value object commands. For information about command priorities, see Command Priority Levels.

Table 1. Binary Value Commands

Name

Description

Operator Override

Replaces Present Value (Appears as O1) at the Operator Override priority with the value you enter in the command. The override has no effect if a higher priority value is in the Present Value attribute.
Note: This command is available only if the Binary Value is prioritized.

Operator Override Release

Releases an Operator Override command.
Note: This command is available only if the Binary Value is prioritized.

Release

Releases a specific priority of Present Value (Appears as O1).
Note: This command is available only if the Binary Value is prioritized.

Release All

Releases Priorities 3 - 15.
Note: This command is available only if the Binary Value is prioritized.

State 0

Releases command Priorities 9 - 15 and then writes State 1 to Present Value (Appears as O1) at Priority 16.
Note: This command is available only if the Binary Value is prioritized.

State 1

Releases command Priorities 9 - 15 and then writes State 1 to Present Value (Appears as O1) at Priority 16.
Note: This command is available only if the Binary Value is prioritized.