Binary Value Object - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This object allows you to hold a binary value for other objects to reference. In the tool, a BV may be created as part of an SAB device to provide binary data points from that device (for example, Temporary Occupancy of the Network Sensor). Alternately, a Binary Value may be created as a reference point for a wireless sensor to write its value (typically to the mapped BV in the supervisory device).

For more information on the Binary Value object, see Binary Value Attributes and Binary Value Commands.