Auto Zero - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Use the Auto Zero feature to calibrate the sensor which is used to measure air flow

The controller performs the Auto Zero feature by overdriving the damper and valve actuators closed for the Auto Zero Duration (in minutes). During this time the Auto Zero Status value is On. When the dampers are fully closed, new values are calculated and stored into the AI offset table in the controller’s nonvolatile memory for Delta P sensors.