Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

An application is a collection of the components that make up the control logic of a system, including modules, logic blocks, custom logic, and hardware definition. The Applications section of the Help system describes the applications as they are presented in the System Selection Wizard and as they are seen in the user interface after being selected.

See the following application sections for details:

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.

See the Configuring a System section for information on how to make selections in the System Selection Wizard.

See the Application Descriptions section for a description of the type of information provided in this Help system for the applications.