Analog Value Object - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This object allows you to hold an analog value for other objects to reference. In the tool, an AV may be created as part of an SAB device to provide analog data points from that device (for example, Zone Setpoint of the Network Zone Sensor). Alternately, an Analog Value may be created as a reference point for a wireless sensor to write its value (typically to the mapped AV in the supervisory device).

For more information on the Analog Value object, see Analog Value Attributes and Analog Value Commands.