The AI object smooths and filters analog data from hardware devices. You can use the value of this object in logic and to monitor the status of hardware.
SAB Device Analog Input objects (for example, network duct or zone sensor AI objects) contain only a subset of the attributes available in Analog Input objects that monitor the hardware inputs of a controller or I/O Module. See the Type column in the table in the Analog Input Attributes section for whether the attribute is present in an SAB Device Analog Input object.
The Analog Input object is reliable when the Present Value is between Min Value and Max Value.
For more information on the Analog Input object, see Analog Input Attributes and Analog Input Commands.