Temperature Control Strategy (SZAHU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Use this section to define the properties of any chilled water or hot water coils. The types of supported coils are proportional or incremental. Entering and Leaving Water Temperature sensors are also supported and add analog inputs for the sensors.